10/12/2017 9:22 AM | |
Posts: 59 Rating:
|
I Have : - S7 1212 Ac/Dc/Relay V4.0 - Tia Portal V13 - Intellisys with Modbus TCP/IP via Ethernet (RJ45) - Modslave App - Modscan32 App I build/set up a MB Client in Network (details in attachment). My remote IP Address is set to my Laptop IP Address. By using Modslave App_with my Laptop IP Address configure in it, I can "Send / Change" the value and my 1212 CPU can read it (in Pointer, starting MW100). My Intellisys is fine and all holding register can be read by Modscan32. But when my S1212 CPU try to Read Holding Register of Intellisys, no luck. I have change the IP Address according to the Intellisys one, but still not work. Please someone help? Thx for you all. AttachmentJpg Attach Zip.zip (876 Downloads) |
10/13/2017 5:06 AM | |
Posts: 59 Rating:
|
No Error at all. |
9/17/2018 3:12 PM | |
Joined: 2/16/2011 Last visit: 1/13/2025 Posts: 229 Rating:
|
Thanks, it solved my similar problem. |
Gabriel de Oliveira |
|
8/22/2022 7:02 PM | |
Joined: 10/18/2016 Last visit: 4/6/2024 Posts: 2 Rating:
|
Hello how to unlok the block becouse is protected |
Follow us on