5/14/2019 9:02 AM | |
Joined: 7/18/2016 Last visit: 2/27/2024 Posts: 23 Rating:
|
hello sir, i want to read data from a converter in modbus tcp/ip i have used mb client in block but i am getting the error 80c8 i have seen the post regarding that error but it was not much helpful i have tried changing the address and,changing the id but nothing happening i also used TCON block to check weather connection is being establishing or not but in that block i am getting error 80a3 i have searched for that also but i find not find the solution if you could please help me Product used 1214C DC/DC/DC-plc software used -TIA v 15 SP1 SC10E4NIM-converter(third party)-which converts modbus RTU to TCP/IP Status: PLC to modscan as server working plc to modscan as client not working converter to modscan working converter to plc not working
AttachmentAYUSH TESTING.zip (85 Downloads) |
5/14/2019 12:00 PM | |
Posts: 1283 Rating:
|
I am not using SP1. Did you changed the MB Unit ID and checked and made sure your CON ID is unique? |
5/15/2019 7:48 AM | |
Joined: 7/18/2016 Last visit: 2/27/2024 Posts: 23 Rating:
|
yes sir my connect id is 1 and my mb unit id is also 1 i have tried changing but it still does not work |
Follow us on