8/10/2022 11:16 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi hubertluczak, how do you change the name of the blocks? Have you only renamed the blocks in the symbol table or with the function "Rewire"? The function "Rewire" rename the block and adapt the new block number at the internal calls in other blocks (also in the blocks that are know protect like APL or Modbus library). More details of the function "Rewire" can be found in the FAQs Rewiring in STEP 7 and Notes on rewiring operands. If you rewire the Modbus blocks consider the FAQ Which blocks for Modbus/TCP can you rename or re-wire when the block numbers of the Modbus blocks are already being used in the user program? With regards |
This contribution was helpful to2 thankful Users |
8/26/2022 8:57 AM | |
Joined: 10/21/2016 Last visit: 11/4/2024 Posts: 49 Rating: (0) |
Thanks, I didn't know that option! |
Follow us on