4/7/2017 7:57 AM | |
Posts: 7 Rating:
|
Hello, from recent time I have a problem with modbus TCP block in TIA Portal 13 SP1. In my old projects, when I pull it from the Communication->Others->MODBUS TCP->MB_Client, it had IP Octet filed where I write address of a device from which I want to read data. Now, after some update, it is different and it don't contain IP filed. I change versions of MODBUS TCP and Open user communication block to same version but the block stay the same. Old block look like this: see attachment New block: see attachment So, I need help to return my old MODBUS TCP block or use new one (to find where to put IP address). Thanks in advance, Marin AttachmentOld_And_New_Block.zip (81 Downloads) |
Last edited by: Min_Moderator at: 4/7/2017 9:04:25 AMAdd attachment |
|
4/7/2017 8:04 AM | |
Posts: 7 Rating:
|
Thanks for the fast replay. You can find zipped images in attachment. Attachmentmodbus.zip (83 Downloads) |
4/7/2017 2:25 PM | |
Posts: 7 Rating:
|
Unfortunately, I still don't know where to put IP address. Do you have any other solution? Best regards, Marin |
Follow us on