12/9/2016 7:53 PM | |
Posts: 26 Rating: (0) |
Here is the picture of timer. Thank you |
12/9/2016 10:30 PM | |
Posts: 5225 Rating: (1194) |
Hi. * No need to close the connection. * No need to set-up a 2nd connection. * Use the outputs of the block to determine when to switch to a new exchange. * Consider using the newest version of Modbus TCP instruction that your PLC can handle. Without trying to cover everything you need for the job and not trying to be 100% accurate - review the attached PDF. The same version instructions vwere used as what you are using. Greetings. w AttachmentDesignIdea_Modbus Client Cascade.pdf (480 Downloads) |
This contribution was helpful to2 thankful Users |
12/10/2016 9:32 AM | |
Posts: 26 Rating: (0) |
Thank you very much on your reply. I will try this on as soon as possible, and give you feedback how it went. Thank you one more time :) |
Follow us on