9/24/2014 6:17 PM | |
Joined: 9/24/2014 Last visit: 10/7/2024 Posts: 2 Rating:
|
Hello, we want to useSIMATIC ET 200SP packed with IM 155-6 (6ES7155-6AA00-0BN0) togetherwith AI Energy Meter ST Modul (6ES7134-6PA00-0BD0). As I understandET 200SP has the same CPU as S7-1500 (CPU1511 /CPU1513) and supports PROFINET.PROFINET and Modbus TCP can coexist on the same physical ethernet, of course. Our higher level control unit speaks Modbus TCP only and we use other PACx200 devices that speak Modbus TCP, too. We want to communicate both with PAC and ET 200SP devices using one control unit. Question: Is it possible to get Modbus TCP working on ET 200 SP using standard Siemens packages provided by Siemens, such as the Modbus TCP implementation for S7-1500? Thank you! |
9/25/2014 6:35 PM | |
Posts: 3093 Rating:
|
Hello Gee, yes, the only limitation is the number of supported connections. Regards, Kaulquappe |
Follow us on