12/1/2016 7:11 AM | |
Joined: 12/14/2013 Last visit: 6/10/2022 Posts: 2 Rating:
|
Is there a PC software test client I can use to test modbus TCP connection to S7-1200 PLC setup as a server. |
12/1/2016 9:33 AM | |
Joined: 4/28/2015 Last visit: 2/3/2023 Posts: 9027 Rating:
|
Hello, this STATUS value shows reason, simply in my opinion if STATUS is 7002 then job is processing, only STATUS 0 shows right execution of instruction with result ok. Look to Help of instruction, there is description of STATUS and of course other status values. Look to Communication or Modbus/TCP conference, somewhere are topics about Server implementation on S7-1x00, also DJ has somewhere post his examples/project with different Client/Server implementation. Also Siemens examples can be found with search box in right corner of this page, really I must say don't know now what posts are about that examples, topics are rise every day so better need manually find some topics. Update: link : Modbus TCP and Modbus RTU sample application Hope it will be helpful to you. |
Last edited by: Duris_I at: 12/1/2016 9:36:02 AMWith best regards... |
|
Follow us on