9/28/2018 10:39 AM | |
Joined: 11/26/2015 Last visit: 2/19/2025 Posts: 92 Rating:
|
Dear all, I have a problem regards the modbus Tx message. I was using S7-416H CPU and ET200SP with CM PtP, the modbus communication was setup through CM PtP. I want to read the current measurements of the 3-phase power meter, so I use FB640 and FB641 for programming. Inputs are as shown in the attached zip file . I couldn't get any reply from the power meter, and when I use another to check the message sent, I found the message sent out was "7a df ff ff bf 1d 1e ff". But in my program, the message supposed to be sent out should be "0b 04 75 31 00 20 xx xx". I couldn't find the reason. Can anybody help? BTW, where can I check the help file of the Modbus library FBs such like FB640, FB641 and FB642? I couldn't find it through the Simatic help file. Thanks for the help. AttachmentModbus Communication.zip (163 Downloads) |
Last edited by: kevinlin_5 at: 9/28/2018 11:12:11 AM |
|
9/28/2018 10:41 AM | |
Joined: 11/26/2015 Last visit: 2/19/2025 Posts: 92 Rating:
|
Image file 3 |
9/28/2018 10:41 AM | |
Joined: 11/26/2015 Last visit: 2/19/2025 Posts: 92 Rating:
|
Image file 4 |
Follow us on