5/21/2013 9:00 AM | |
Posts: 168 Rating:
|
Hi Guys and Gals, I'm new to Modbus with a Siemens system, I've done several Modbus communications with other systems before. But, Siemens doesn't look the least similar to what I'm used to I've checked the example code provided here and find it quite useful, but I have a few questions. Can I use a DB selected by me for the data transfer, in HW config somewhere ?? Where do I specify what DB I'd like to use for the data exchange, HW config ?? Is it possible to use one DB for TX and another for RX ?? Do I need to specify the length of the transmission and reception ?? Cheers |
Last edited by: O_Moderator at: 5/27/2013 9:50 AMnew subject after splitting from /tf/WW/en/Posts/72742#top |
|
5/31/2013 10:37 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Hello Bryll; Sorry if this is unnecessary, but before step 1 in your list there is another importantstep: Purchase of the correct license for Modbus RTU, and insertion of the hardware dongle (included in the driver delivery package) in the slot at the back of the CP 341 you are using in the project. Which drivers can be loaded for the serial communication processors? What should you watch out for when programming the communication blocks for Modbus S7-300 CP341 as a slave? If this step has been taken care of already, please give us more information about the "wrong software to initialize the module" that you downloaded, and on the driver you believe you need now and cannot find. Maybe we can help. Loadable Driver Modbus Slave (RTU) Download CD "CP340, CP341, CP440, CP441" Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/31/2013 10:37 PM |
|
This contribution was helpful to
1 thankful Users |
6/11/2013 12:52 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Hello Bryll; And welcome to the world of Siemens PLCs... Daniel Chartier |
Follow us on