11/11/2016 12:03 PM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello All,
AttachmentModebusPN.zip (88 Downloads) |
11/11/2016 1:09 PM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello DJ_1 The ModSIM looks connected to Port 502 - PLC. The ID is 1, Address 0100, Length 100. But all Data are on 0. |
11/14/2016 1:20 PM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello DJ_1 The Port an Device is 42001. If I type this Number in, then I get an Error: Please enter an integer. |
11/14/2016 3:53 PM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello,
|
11/15/2016 8:48 AM | |
Joined: 6/4/2013 Last visit: 1/6/2023 Posts: 52 Rating:
|
Hello DJ_1 I attached my test Project. I have now an Error A093. The PLC (IM151-8) is Client. In DB2 I have: local_tsap_id 502 rem_tsap_id 502 (Device have Port 502, the 42001 is Service Port for Device) IP of Device 192.168.1.50 "CONTROL_STATUS".CONN_ESTABLISHED is on true, BUSY and ERROR are flashing - Error: A093. AttachmentModbusPN_PLC_is_Client.zip (81 Downloads) |
Follow us on