9/10/2015 5:35 PM | |
Joined: 7/19/2011 Last visit: 1/21/2025 Posts: 262 Rating: (5) |
Dear all I am doing a RS232 communication with a Minilec Annunciator in Wincc TIA V13 SP1 advance. First i am checking the same in modscan with Station Id 1 with 9600 baudrate and 8 word length , Even Parity and 1 Stop Bit. I am getting the data as Input Status from 10001 to 10032 in Modscan. after that Same thing i am trying in Wincc TIA V13 with same Station Id and same Com port settings, but i am not getting any data. Kindly check attachments for screenshots. Also one more RS232 communication i am trying with L&T Vego series Energy meter, here i am getting data in 40000 series (Holding Register) adresse's but in 30001 series address i am not getting any data but in modscan data is there for 30000 series . Kindly help AttachmentModbus Communication.zip (241 Downloads) |
JAVED AKHTAR |
|
Follow us on