6/26/2012 5:05 PM | |
Joined: 1/17/2007 Last visit: 3/10/2025 Posts: 1557 Rating:
|
According to the manual it can handle either RS485 or RS422. Electrically RS422 and RS485 are the same. The only difference is that RS485 has tri-stating traansmitter control. So using the manual as my only source of data, as I have never seen or used this convertor myself, it would appear that it should work. The only way to be sure is to try it. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to
1 thankful Users |
Follow us on