8/31/2010 10:06 PM | |
Joined: 4/29/2009 Last visit: 3/7/2025 Posts: 13 Rating:
|
Is it possible to modify the IP addess of a PN CPU dynamically? (perhaps from an HMI?) |
9/1/2010 9:11 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hi, I'm sorry this is not possible because the IP-Address is part of the Step 7 program and included in the SDB's which can only be changed by Step 7. When you use a CP343 which supports the configuration of the CP from the user program this is possible. More can be found in the following FAQ: How can you configure an S7 CP during runtime? |
Best regards, |
|
9/2/2010 1:09 AM | |
Posts: 5822 Rating:
|
Hello all together, may I interrupt here for a second. I know this feature is rather new, but it is called Mini_IP_CONFIG. It is part of STEP 7 V 5.5 and the brand new CPUs. The function allows the required feature. For more details please contact your local distributor. You may also check here. Best regards J_Bell |
This contribution was helpful to
1 thankful Users |
Follow us on