7/20/2011 2:30 PM | |
Posts: 41 Rating: (1) |
Hi, I'm using the PCS7 AP Library for the first time. On the MonDil block (Digital Input), my alarm is activated when the input is "1". How do I reverse this? |
7/20/2011 3:10 PM | |
Posts: 50 Rating: (1) |
Hi Tuff, |
7/20/2011 3:10 PM | |
Posts: 50 Rating: (1) |
Hi Tuff, |
7/20/2011 3:53 PM | |
Posts: 41 Rating: (1) |
I want to avoid this. Isn't there a bit on the block that I need to set or reset? |
7/20/2011 5:00 PM | |
Posts: 836 Rating: (99) |
Can you please upload a screentshot of the mondil block with its interconnections. |
7/21/2011 7:17 AM | |
Posts: 50 Rating: (1) |
hi, feature bit 22 setting you can see there......... |
7/21/2011 9:34 AM | |
Posts: 41 Rating: (1) |
Hi, Feature Bit 22 doesn't seem to work. I still get an alarm on an input state of "1". |
7/21/2011 9:56 AM | |
Posts: 50 Rating: (1) |
Hi, Compile entire OS and check for it it should work.....................after changing the feature bit22 |
3/31/2020 6:07 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Yes, you still need a not gate to inverse the input. I personally hope that they can have a inverse feature bit too, but no, they do not have. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on