5/1/2012 9:17 AM | |
Joined: 3/14/2008 Last visit: 9/27/2024 Posts: 2098 Rating: (938) |
I think you need to use communication blocks like BSEND,BRCV,TRCV,TSEND,blocks for your important data...and display this in the OS of the AS (s7400)... |
If I could help you, you can use the RATE button. Thank you. |
|
5/1/2012 9:18 AM | |
Posts: 691 Rating: (37) |
HI Behrooz You can merge the S7-300 project in the PCS7 and work with the project Make two Connections in the WinCC Tag Management You have to copy the PDLs(you may have to reassign the Tags in the Pdls) |
Follow us on