Industry Online Support
Technical Forum
10/27/2010 1:00 PM | |
Posts: 3 Rating:
|
Hi. Is there any way to have more then one email address in WinCC flexible, or the possibility to use a internal string to edit the email? Thx. //Tommy |
10/28/2010 6:32 PM | |
Joined: 7/28/2010 Last visit: 7/16/2023 Posts: 184 Rating:
|
Tommy, You should be able to create a script and call "Send Email" to send more than one email. If that doesn't work then you can define an internal tag and connect that to an Input/Output fieldso you can editthe email address. Regards, Behnam www.sigmaprocess.ca |
10/29/2010 8:26 AM | |
Posts: 3 Rating:
|
Thanks for your answer, but how do I trigger the script when there is an alarm? BR Tommy |
10/29/2010 1:57 PM | |
Joined: 7/28/2010 Last visit: 7/16/2023 Posts: 184 Rating:
|
Tommy, 1. You can call the scriptevery time the alarm Screen gets activated. Go to "Alarm View\Events\Activate" and call the script. 2. If you want to send an email for a specific alarm. You can call the script when the Tag changes value. Go to"Tag\Events\Change Value" and call the script. Regards, Behnam www.sigmaprocess.ca |
Follow us on