3/7/2018 6:37 AM | |
Posts: 69 Rating: (4) |
Thank You for your valuable help! One more help is needed. When pressing the run push button, ie, when the drive starts, motor should run at a speed of 10 rpm. Please help me with that too. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/14/2018 10:03:52 AMNew subject after splitting |
|
3/7/2018 7:45 AM | |
Posts: 69 Rating: (4) |
p1070 is the main setpoint.How can we use it to the min speed? |
3/7/2018 12:38 PM | |
Posts: 69 Rating: (4) |
so will the drive start if i press this 10 rpm PB? ie, what will be the condition of p0840? |
3/8/2018 8:24 AM | |
Posts: 69 Rating: (4) |
But, how can I use use jog mode and motp together? Jog should be stopped before using other parameters.Right? |
3/8/2018 8:29 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (880) |
What I am suggesting is, use JOG mode to run motor at 10 RPM. For 50-600 RPM you can use MotP. |
Follow us on