1/15/2009 1:57 PM | |
Joined: 3/21/2006 Last visit: 1/13/2025 Posts: 10239 Rating: (1182) |
Hello tbe, You have physically copied a STEP 7 project with a PC station and OS (Operator Station) configured in it onto another (new). computer. You have then tried to load the OS using SIMATIC Manager. For more details and warnings look at The XDB file with the PC station configuration can no longer be found after copying the project to another computer If you have some troubles next links could help... Creating an XDB file for an Ethernet SoftNet card with STEP 7 V5.x + What remedies are there when you can't load the configuration of the PC station? |
Follow us on