5/27/2016 9:50 PM | |
Posts: 7 Rating:
|
Hi, I have big problem I have MP 277 10" Touch Panel, I restore my back up on it by Prosave V13 but the HMI hung on Bootloader MP 277-10 Touch Version 1.1 Date: 19.10.2006 And I switch off the power and switch on but still the problem. Could you see attachment. Help plz. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/30/2016 12:34:53 PMNew subject after splitting |
|
5/28/2016 5:49 PM | |
Joined: 3/28/2015 Last visit: 2/15/2025 Posts: 722 Rating:
|
Hello, Kindly follow the following procedures: 1- OS update: How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?Which connector cables are available for connecting to SIMATIC Panels?2-Restore the program image into the Panel using ProSave software.
|
Eng.Mohamed Ibrahim |
|
Follow us on