11/5/2015 4:32 PM | |
Posts: 9 Rating:
|
I am using MP377 12" touch screen, since long time its touch screen not working so using USB device we are running machine. So what is the procedure of calibrating the touch screen & if I calibrate, is there is any need to load HMI program ? Also it is having one CF card so backup of HMI is stored in card? I am asking this because we are not having backup of HMI program. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/8/2015 11:10:52 PMNew subject after splitting |
|
11/5/2015 8:35 PM | |
Joined: 3/28/2015 Last visit: 2/15/2025 Posts: 722 Rating:
|
Hello, 1-Calibrating the touch screen not affect on the program stored in the panel. Kindly find the attached file. 2-If this not solve the problem, Do the following: What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? |
Last edited by: The Helping Hand at: 11/6/2015 12:05:27 PMReplaced the link by a static one Eng.Mohamed Ibrahim |
|
Follow us on