9/13/2016 9:47 AM | |
Joined: 4/24/2006 Last visit: 4/23/2025 Posts: 8965 Rating:
|
Hello prabhakaran, Please have a look at the following link: SIMOTION SIMOTION SCOUT SIMOTION SCOUT TIA device proxy You will have to synchronize the HMI tags. See page 38 and 39 of manual. (You can download from above link) Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
9/14/2016 2:08 PM | |
Joined: 6/18/2012 Last visit: 2/10/2025 Posts: 35 Rating:
|
Hello, Finally i have got one manual Regarding Device Proxy on Simotion controllers in TIA portal. So follow the above link to create Device proxy connect the Simotion controller but I con't resolve the connection tag error. Our Last discussion you suggest the tag synchronization, which is also done kindly support further. Here I have attached the program Backup for your ref. Thank you Regards, Prabhakaran D AttachmentBackup.zip (112 Downloads) |
Follow us on