12/18/2017 12:34 AM | |
Posts: 2 Rating: (0) |
Hi i have same problem with 2 mp277 8" touch one of them is in secure mode(control panel password protection )and another Defective Operating System i tried all the suggested ways to make os update (when i choose my hmi type the factory reset goes to hidden so i can not chose it). i have the source so i can make factory reset . but how???? what can i do? trow may panel out? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2017 12:15:09 PMNew subject after splitting |
|
12/19/2017 2:39 PM | |
Posts: 11 Rating: (0) |
Hello Autogen, Are you try to make the Factory Reset using ethernet port? because is not possible to make a Factory Reset using ethernet you must use PPI cable. take a look here: |
Last edited by: INGELM at: 12/19/2017 2:47:56 PMLast edited by: Jen_Moderator at: 12/21/2017 9:17:09 AMInserted right link. |
|