Industry Online Support
Technical Forum
4/17/2013 1:41 PM | |
Posts: 3037 Rating:
|
Hello, If you use logging in a text file then you must use the function "Close All Logs" or The function "StopRuntime ". The logs are closed right with this function. If you pull the voltage plug, then the logs are not closed correctly. You have data loss and the log can bedamaged. Do you have problems with voltage? See the first note the attachment. How are tags and alarms logged in WinCC flexible? Then you should use an UPS. How can you ensure safe shutting down of the Panel Runtime on a Windows-based operator panel if there is a power failure? Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on