2/19/2014 7:48 PM | |
Posts: 8946 Rating:
|
"I know the best is the RS232 Multimaster " Bad chance without, I am afraid. |
2/20/2014 7:34 AM | |
Joined: 4/22/2010 Last visit: 2/26/2025 Posts: 5697 Rating:
|
Hello, You have to perform an operating system update with reset to factory settings if the HMI device does not yet have an operating system or if the HMI device's operating system is corrupt. See attachment for instructions. Regards, Marcjan AttachmentOSupdate_with reset.pdf (1069 Downloads) |
Problem solved? |
|
This contribution was helpful to
4 thankful Users |
2/20/2014 6:07 PM | |
Posts: 8946 Rating:
|
But "reset to factory Settings" will only work with multimastercable, right? |
2/20/2014 8:05 PM | |
Posts: 8946 Rating:
|
That comes with ProSave |
2/20/2014 8:07 PM | |
Posts: 11 Rating:
|
Oh I searched the folders for a .img file but nothing came up. I downloaded the software from the site but any ideas where it would be? |
2/20/2014 8:34 PM | |
Posts: 11 Rating:
|
Oh I only have ProSave not Wincc Flex so maybe that img file doesnt come with Prosave? I searched but couldnt find it. |
Follow us on