Industry Online Support
Technical Forum
9/8/2009 7:50 AM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Hello Fred, Look at How do you integrate an operator panel into a local network? IP address of panel should be from the same "family" like existing network. For example if IPs into existing network begin with 177.10.1.xxx, panel should heve 177.10.1.xx1. The IP of panel mus be unique, also all existing IPs there. Subnet mask must be the same for all IPs. I guess you'll use switch to connect panel to existing network. The necessary cable is "straight" type. Into Google you can find more info about this cable. Hope this will helps. Best regards, Hristo Mihalev |
Follow us on