Industry Online Support
Technical Forum
6/13/2012 10:04 AM | |
Posts: 1547 Rating:
|
1) Do you have to use more than one AP which means that the the MP has to change between the different APs (Roaming)? If yes you will need the iPCF-MC functionality which is only provided by Siemens RR-APs. 2) There is an application example which explains the behaviour of the system if the MP leaves the area of the AP. It depends on your program: Always make sure that the signal strength is sufficient. If the radio link quality is too poor, a “global rampdown” is initiated. Depending on the created program, a defined slow stop of the associated machines is executed in the F-program. |
Last edited by: Rated X at: 6/13/2012 10:06 AMLast edited by: Rated X at: 6/13/2012 10:05 AM |
|
Follow us on