Industry Online Support
Technical Forum
5/2/2011 3:56 PM | |
Joined: 12/1/2006 Last visit: 9/5/2023 Posts: 26 Rating:
|
WinCC flexible also a bit of the PLC from the Windows Media Player I know how to operate |
5/2/2011 4:08 PM | |
Joined: 4/29/2010 Last visit: 9/21/2023 Posts: 1557 Rating:
|
Hello, your discribtion is very strange best regards |
5/3/2011 7:49 AM | |
Joined: 3/21/2006 Last visit: 7/12/2023 Posts: 10221 Rating:
|
Hello, Perhaps might helps - How do you start a sound file via a script in the WinCC flexible PC Runtime? Best regards, Hristo Mihalev |
5/5/2011 4:16 PM | |
Joined: 12/1/2006 Last visit: 9/5/2023 Posts: 26 Rating:
|
Doing a simulation of the car. WinCC flexible Runtime is running a simulation of the car, brake or clutch pedal is pressed from the outside in WinCC Runtime want to play the appropriate sound. When pressed a button in WinCC Runtime running the sound I know. However, depending on the audio file does not work with an external switch. I wrote the script works, but once running. Page after you install the brake pedal is pressed the script does not work AttachmentDesktop.zip (26 Downloads) |
Last edited by: huseyin_x at: 5/5/2011 4:17 PM |
|
Follow us on