Industry Online Support
Technical Forum
3/30/2007 3:16 PM | |
Posts: 1275 Rating:
|
Hi Did you use flexible or pro tool for the application? Which funcionallities does it have? The MP's each lock up at independent random times, right? |
4/2/2007 11:03 AM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi, maybe you use a CF card that is not released for the panel. That could be a reason for that problem Bye |
4/27/2007 2:41 PM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating:
|
Hi, I've seen these things with OP/TP27 and OP/TP270, programmed with ProTool. The only persons who could repair this software problem where thoseguys/girls from the ProTool developing department, because there was something in the structure of the project that cannot be repaired with simple ProTool. I suggest you open a Support Requestand include your project file with it. |
Smurf |
|
Follow us on