Industry Online Support
Technical Forum
11/6/2014 12:27 PM | |
Joined: 11/21/2007 Last visit: 12/23/2024 Posts: 2325 Rating:
|
Hello pobrien The Operating Temperature of MP377 ( As per ST80 Catalog ) is 0-50 Degree C. So you should not have any problem as far as the temperature is concerned. You should however is careful about Condensation ( Inside the MP ) at low temperatures as that is quite harmful for the unit. Humidity level should not exceed 90% to avoid condensation. Cheers Navnag |
There is no such thing as the last bug in a program |
|
11/6/2014 2:29 PM | |
Posts: 1058 Rating:
|
Hello probrien, I can only agree with Navnag. The problem at such low temperaturewill be condensation. But I would rather keep humidity below 80%. regards |
This contribution was helpful to
1 thankful Users |
Follow us on