3/20/2014 8:53 AM | |
Joined: 5/15/2012 Last visit: 5/21/2024 Posts: 39 Rating:
|
I have MP 377 with visualization created in WinCC flexible 2008 SP3. Panel has IP address 172.16.76.221 and subnet mask 255.255.255.0. I need send created file to server with IP 172.16.2.186. On server is created shared folder (access with name and password). I used name of server no IP address for path of connection with server (How do you integrate an HMI operator panel into a local network?). Problem is MP 377 can’t create file on server. If I tried creating file on my PG (Windows XP SP3) with IP 172.16.76.200 (same subnet) it was without problem. I used name of PG no IP address. I tested ping from MP 377 to my PG and to server: - ping IP address to PG no problem - ping name to PG no problem - ping IP address to server no problem - ping name to server without success I tried: set DNS server this look good but I don’t know how change register in MP 377 (Windows CE 5.0) http://windowsmobilepro.blogspot.sk/2006/04/etchosts-file-equivalent-in-windows.html I tested but don’t work (absent some component) http://geekswithblogs.net/BruceEitman/archive/2009/07/27/window-ce-simple-little-registry-editor.aspx
I need know it possible created file in another subnet. If YES how. Thanks :-) |
3/24/2014 4:32 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello Palo, i think first of all you should take a look at this FAQ wich explains the possible ways to include a panel in a network (also the file exchange to a sharded folder): How do you integrate an HMI operator panel into a local network? With best regards |
Follow us on