1/17/2016 10:31 PM | |
Joined: 5/3/2015 Last visit: 2/18/2025 Posts: 1 Rating:
|
Hi all, I have a problem with a MPI Communication. In the project attached, I don't understand the exchange MPI. I have 3 PLC and : * PLC_LAVAGE exchange with 11GH0001 : DB30 => DB31 * PLC_LAVAGE exchange with 21GH0001 : DB30 => DB31 * PLC 11GH0001 exchange with PLC LAVAGE : DB31 => DB31 or DB32 * PLC 21GH0001exchange with PLC LAVAGE : DB31 => DB31 or DB32 Where is the code for the exchange ? I don't understand. For Profibus, That's OK. FC100. Thanks, Eric AttachmentFAP.zip (59 Downloads) |
Follow us on