9/21/2009 8:54 AM | |
Posts: 10 Rating: (0) |
Help!! , MPI network connecting PLC S7-412 (Master) with 3 x S7-314 and some other equipment (see attachment). After I turn the S7-400 off and then on again, everything look's OK but I cannotconnect to the slave S7-300 stationsvia the MPI Network. Only Downloading the HW configuration of the S7-400 solves the problem. AttachmentSinchro_current.zip (122 Downloads) |
9/22/2009 5:09 PM | |
Posts: 5822 Rating: (412)
|
Dear Felman, I am not sure but is it possible that you have a CPU FW < V 4.1.0 with your S7-412-2 CPU? If so please update to: Firmware Updates for S7-412 CPUs V 4.1.1. It may fix a problem, especially if you access unavailable IO with your panels. Best regards J_Bell |
Follow us on