3/10/2011 7:37 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Look at attachment. For me is strange why do you have this symbol there. Seems you are working under Windows7 (hope 32bits platform) and this symbol there is a part from Windows protection messages. This kind of messages are receiving in Win7 if you try to start a program or install a new software. Try with disable this messages. Go on Control Panel -> User Account Control Settings (look at attachment). Also disable Kaspersky anivirus program. Perhaps someone has another ideas. Best regards, Hristo Mihalev Attachmenttestr.zip (237 Downloads) |
3/10/2011 7:58 AM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
Dear UMENCHO, I have tried those steps but invain Help. Tomy. |
Aim Higher |
|
3/10/2011 8:46 AM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
By the way, I have refered to the device manager and it showed that adapters are there and installed. Also I have checked regitry files and it seems that every thing is OK (as far as i know) Please check attached. Any ideas I will be more than greatfull. Tomy. AttachmentAdapters.zip (268 Downloads) |
Aim Higher |
|
3/10/2011 8:52 AM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
Dear UMENCHO, Would you please provide me with registries of "PC Adapter USB" and "PC/PPI". Regards. |
Aim Higher |
|
3/10/2011 9:07 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi Tomy Master, If it´s possible go backwards by system restore point, if you remember when this interface last timewas ok. How about last windows updates/other updates or software installationsis there some connection. This windows icon in Set PG PC interface might mean that some security programsettings controlling this program (firewall etc.). In my PG there is not this kind icon. Are you admin in this programming unit. You allready answered this last question -Heksu- p.s. "The following compatibility list gives the compatibility of the different versions of the SIMATIC software packages with the last two versions of STEP 7 and with the various Microsoft Windows operating systems. The list is valid only for the versions given in these files" AttachmentSTEP7_Compatibility_en.pdf (151 Downloads) |
Last edited by: Heksu at: 3/10/2011 9:31 AMLast edited by: Heksu at: 3/10/2011 9:10 AM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
3/10/2011 9:41 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Exactly, this is the problem. Look at attachment about setting for PC Auto and MPI, I don't have PPI. Best regards, Hristo Mihalev Attachmenttesty.zip (151 Downloads) |
3/10/2011 10:18 AM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
Dear UMENCHO, I went there and I did not find it, do you recomment to import it? Regards. Tomy |
Aim Higher |
|
3/10/2011 10:25 AM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
I have disabled both firewall and kaspersky, yet it won't accept to install it |
Aim Higher |
|
3/10/2011 10:31 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Yes Tomy to importthem manually. |
This contribution was helpful to1 thankful Users |
3/10/2011 11:04 PM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
Dear UMENCHO, Hallelujah I have restored my interfaces by importing them manualy Thank you all. Tomy. |
Aim Higher |
|
Follow us on