10/9/2007 5:52 AM | |
Joined: 5/25/2007 Last visit: 11/7/2023 Posts: 83 Rating:
|
Hello: Best regards Buzz LightYear Attachment20071009_Diagnose.zip (23 Downloads) |
10/9/2007 7:20 PM | |
Posts: 1275 Rating:
|
Hi, In your logs I found a coupls of access violation entries, like: // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 8.10.2007 - Time: 7.8.38 // Caused at logical address 77BFA573 01:00019573 //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 8.10.2007 - Time: 7.20.59 // Caused at logical address 01D12B1F 01:00001B1F //==================================================================== // FAULTING MODULE: C:\Program Files\Siemens\WinCC\bin\SIMATIC S5 ETHERNET LAYER 4.chn //==================================================================== //==================================================================== // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 08.10.2007 - Time: 07:28:21 // Caused at logical address 00429ADA 01:00028ADA //==================================================================== // FAULTING MODULE: C:\Program Files\Siemens\WinCC\bin\pdlrt.exe //==================================================================== I've found another thread from you, with the same access violation problem. Is this still the same station? So... you should check those out! This thread may help. Also... you could upgrade your system to v6.0 SP4, which would provide more stability. Best regards, Danielle |
10/19/2007 10:44 AM | |
Joined: 5/25/2007 Last visit: 11/7/2023 Posts: 83 Rating:
|
Dear Danielle: Best regards Buzz LightYear |
Follow us on