10/31/2023 12:05 PM | |
Joined: 2/3/2022 Last visit: 4/23/2024 Posts: 304 Rating:
|
Hi! Could you share some screenshots? In any case, you can always open a Support Request with those questions. Br! |
10/31/2023 12:26 PM | |
Joined: 7/19/2022 Last visit: 4/23/2025 Posts: 436 Rating:
|
Hello Rusbi, To create a new recipe you must set the value that you want each element of the recipe to have and enter the ID that you want that new recipe to have (for example through a tag in an I/O field). Using the "LoadAndWriteParemeterSet" event, you must select the ID of the parameter set type and use the ID that you assign to it in the tag mentioned before. Then you must save it with the "ReadAndSaveParameterSet" event reading the same parameters as before. |
If this Information really helps, you could use the Rate function |
|
Follow us on