8/26/2008 4:17 AM | |
Posts: 32 Rating: (0) |
Thanks But not clearly understood. Please explain as how applicable in my case (multi user). Any documents available?????? Or any other example for it. Regards, Dip |
8/26/2008 8:46 AM | |
Posts: 102 Rating: (11) |
Hello Dip!! I think what you want to do is a project with more than one PLC connected... am I right? If I understood well, in your project, there is only one PC, that would be a single-user project. The multi-user projects are projects which have more than one PC controlling a plant (with "n" number of PLCs), so, unless your project has more than one PC controlling your both systems (plant and boiler),you need asingle user project. Now what you need to do is to set up the connections to both systems, and this depends on the communication protocol that you are using (e.g. MPI, PROFIBUS, PROFINET, Ethernet...). Usually you do it through the S7 Protocol Suite. I am attaching to you a document from Siemens where shows how to make a first project, it can explain you how to make a first connection If you have any more questions, let us know Attachmenthmi_wincc_v6_2_getting_started_en[1].pdf (205 Downloads) |
8/27/2008 8:53 AM | |
Posts: 102 Rating: (11) |
Hi Dip!! AttachmentPicutres add Profibus driver.zip (76 Downloads) |
This contribution was helpful to1 thankful Users |