10/16/2008 2:56 AM | |
Posts: 5 Rating: (0) |
How to create a multiplexing of variables in the WinCC SCADA |
10/16/2008 9:10 AM | |
Posts: 102 Rating: (11) |
Hi Juanjose! |
10/16/2008 11:17 AM | |
Posts: 1776 Rating: (95)
|
Hi, explain a little bit more what you like to do |
10/16/2008 5:29 PM | |
Posts: 5 Rating: (0) |
In the multiplexado, that is a type of indirect addressing the used variable is only determined in runtime. For the multiplexada variable a list of variables is defined. From the list of variables the relevant variable in runtime is selected. The selection of the variable depends on the value of the index variable. In runtime the first one reads the variable value off the index. Next it is acceded to the variable that is in the pertinent position of the list of variables. Attached image Juan José Ramirez From: Puebla, Mex AttachmentMultiplexar.zip (68 Downloads) |
10/16/2008 6:48 PM | |
Joined: 9/28/2005 Last visit: 5/23/2024 Posts: 2957 Rating: (242) |
So what's the question ? |
Best regards, |
|
10/16/2008 7:08 PM | |
Posts: 168 Rating: (49) |
I deserve more money ... and chicks and other cool stuff hum heh heh hum heh |
Last edited by: DimiCamp at: 10/16/2008 7:10 PM |
|