Industry Online Support
Technical Forum
4/17/2012 12:02 PM | |
Posts: 3037 Rating:
|
Hello, You can create a message view with systemmessages in WinCC flexible or ProTool. Now you can see a systemmessagein this messageview if the connection to your plc is lost. Do you checkwhether you have problems with EMC in your plant? Electromagnetic compatibility Tweety |
4/18/2012 11:03 AM | |
Posts: 3037 Rating:
|
Hello, Yes, you can download your project new. You should clear your panel about an OSupdate with the option "reset to factory settings". How do you do an operating system update (OS update) on operator panels? Then you can download your project to your MP270. Or you download abackupwith Prosaveto MP270. MP270 has the operating system WinCe 3.0. You can not do an update of the operating system from WinCe 3.0 to WinCe 5.0. Tweety |
Follow us on