6/8/2022 5:51 PM | |
Joined: 12/18/2014 Last visit: 12/6/2023 Posts: 31561 Rating:
|
Please upload your program as a ZIP file. |
6/8/2022 6:58 PM | |
Joined: 9/23/2021 Last visit: 4/13/2023 Posts: 9 Rating:
|
Hi, thanks for answering my call. The counter "A" is the B001 displayed at the bottom of the display. The counter "B" is B009 displayed vertically with B041 and B047. What I am trying to realize here is a 3 stage counter that turns on a relay at a given setting. AttachmentCount-loss-tests.zip (240 Downloads) |
6/9/2022 4:46 AM | |
Joined: 12/18/2014 Last visit: 12/6/2023 Posts: 31561 Rating:
|
The cycle time depends very, very much on the program used. The size of the program, the type of blocks used, whether and how much communication takes place with remote devices and which LOGO! is used. Counting fast pulses up to 5 kHz only works when the counter is running. The evaluation of the digital output of the counter now depends on the cycle. So I can't offer you a solution for your problem. AttachmentCounting more then 999,999.zip (205 Downloads) |
Last edited by: ixo65 at: 06/09/2022 04:57:26 |
|
This contribution was helpful to
1 thankful Users |
6/9/2022 4:30 PM | |
Joined: 9/23/2021 Last visit: 4/13/2023 Posts: 9 Rating:
|
Thank you for the 1E6 counter circuit! |
This contribution was helpful to
1 thankful Users |
Follow us on