2/13/2017 3:02 PM | |
Joined: 3/28/2010 Last visit: 12/4/2024 Posts: 1090 Rating: (215) |
> it shows the only real difference between the 2-wire mode and 4-wire mode as being the resistors, but there is more resistance on the 2-wire. Each 250 ohm resistor (on the ones/tens numbered wiring terminals) is effectively directly across the input of the amplifier (the triangle) on the twenties/thirties number wiring terminals. It is there to create an IR drop of 1-5Vdc that the amplifier can 'see'/'read'. |
2/14/2017 3:29 AM | |
Joined: 3/28/2010 Last visit: 12/4/2024 Posts: 1090 Rating: (215) |
We'll never know how it works because the diagram on pg 372 is just a vague block diagram, unlike the other diagrams that were very explicit. However, the "Measuring range Modbule setting is clearly part of the equation. https://s7.postimg.org/6p1ss192z/measuring_Range_module_setting_determines_2_wire.jpg C mode or D mode is the determining factor as to whether the external DC supply is switched to the 2 wire transmitter (+) or whether it is not switched for a 4 wire transmitter and for the 'routing of the DC (-) return, even though how all that is accomplished is not revealed. |
Follow us on