4/7/2016 4:52 AM | |
Posts: 70 Rating: (0) |
Dear All, Can u show me when i did : Using Simatic Automation License Manager-> Select Edit->Connect Target System-> Connect AS410 and connect to desired CPU, but my CPU is grey out, I cannot choose it to do anything Please look picture attached. Thank you so much. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/7/2016 9:38:42 AMNew subject after splitting |
|
4/7/2016 7:23 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Goodmorning! So you have opened Automatic License Manager did the following: Select menu Edit->Connect Target System->Connect AS410 and then you clicked on "Add"? In there you can select your multiproject, make sure "Component View" is set and please click on "K1" instead of "2014Q112_Prj". It should be possible to select the CPU in the right column. |
If I could help you, you can use the RATE button. Thank you. |
|
4/8/2016 3:37 AM | |
Posts: 70 Rating: (0) |
Yes, I did like that, I don't know why it still becomes grey out. Can anyone give me an advice ? Much appreciate. |
4/19/2016 1:16 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Hi MD_dx, Make sure you have the following requirements: - You are using PCS7 8.1 - You are using the CPU410-5H as of firmware 8.1 If one of these requirements is not met, you cannot update the license. |
If I could help you, you can use the RATE button. Thank you. |
|