9/16/2018 12:31 PM | |
Joined: 6/1/2018 Last visit: 7/8/2024 Posts: 10 Rating:
|
I attach more pictures of the results of the configuration. Greetings! AttachmentNamed Connections.pdf (999 Downloads) |
9/16/2018 2:32 PM | |
Joined: 9/3/2008 Last visit: 3/20/2025 Posts: 933 Rating:
|
OK, You have CP card. Yes, in ES, configure the netcad (CP 16xx) and download it to the server(s). I have attached pictures 01 to 03. Picture 01, is the Properties of the server PC station. The "Name" is the Windows computernam of the OS server. Make sure there is a checkmark in the "Computer name identical to PC station name". I assume you have this correct since it worked before. Picture 02, is the hw config of the server PC station. Here the CP card is inserted and you set the MAC / IP address. You probably also have this since you have netpro connections set up. Picture 03 shows after you have the above points set up and compiled and the connections in netpro correct, then you right-click the PC station and select "PLC -> Configure". This will insert the CP card and WinCC Appl in the Station Configuration Editor in the OS server. After this, you right-click the PC station again and select "PLC -> Download". This will download the configuration of the CP card and connections to the OS server. If the settings of Simatic Shell on the ES or OS is not set correct, the download may fail. Attachmentpcstation.zip (531 Downloads) |
Last edited by: Michael K at: 9/16/2018 2:41:16 PMMichael |
|
9/16/2018 5:25 PM | |
Joined: 9/3/2008 Last visit: 3/20/2025 Posts: 933 Rating:
|
Hi, About picture 01, then add the checkmark. About picture 03, then downloading the PC station from NetPro has the same effect, but see chapter "6.2.3 How to check and modify the configuration" in the following manual: SIMATIC Process Control System PCS 7 Operator Station (V8.2) Check whole chapter 6 "Configuring the OS data in SIMATIC Manager". About address, see page 41, item 7. ISO is recommendoed, but tcpip is also possible. To be able to test via OS Simulation on the ES, follow chapter "6.2 Configuring the communication paths" where you also make a connection from ES to AS ("Configuring the ES - AS connection"). |
Michael |
|
9/17/2018 10:28 AM | |
Joined: 6/1/2018 Last visit: 7/8/2024 Posts: 10 Rating:
|
Hello Michael, About picture 01, we can not do that now since it involves many changes in the system and the process is running and operative (Am i right?). If I check the box it wont be matching the name configured in the project (if I dont have other choice i will do it). However names are the same in the text box defined for that. About ISO, how do I define the MAC ADDR? By looking phisically to the card / checking IP CONFIG in Command prompt? This changes force me to stop the PLC, right? I have noticed that if i make a change in the HW config of a PLC it lets me make the changes in RUN but sometimes my process goes to fault and stops the process even for 1 second even if I have H-System (maybe redundancy problem). Is this normal? I will follow the configuration of the ES in order to test my comms before downloading. Thanks! Regards, |
Follow us on