Industry Online Support
Technical Forum
9/2/2012 1:39 PM | |
Posts: 664 Rating:
|
Hai, Which is the controller you are using?? 810D/840D If you have backup of NC/PLC with you,Just try for PLC&NC clearing. If it is OK, and "6" is displaying after clearing your hardware is OK,and reload your backup. If not,your Hardware may have some error.May have to repair the hardware/reload the system software.. Thanks&Regards, Raj
AttachmentNC_PLC_Data_Clear.pdf (75 Downloads) |
This contribution was helpful to
1 thankful Users |
9/3/2012 8:08 AM | |
Posts: 36 Rating:
|
Hello. It started working. Its good that I had backup... Too bad we will have to classify it as "unexplainable machine bad day". Thans for help everyone.
|
Follow us on