12/8/2018 4:30 PM | |
Joined: 4/4/2011 Last visit: 1/27/2023 Posts: 25 Rating:
|
Hi Bartosz, I am currently working on a project which required the "travel to fixed stop" function. I hope you can share with me how do you achieve this function in Sinamics S120. Currently, I need my axis to turn until it reach a certain torque, for example 1Nm. When 1Nm is reached, the axis will stop and then reference is set. Really hope you can share with me as I am new to Sinamics S120, thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/10/2018 11:28:58 AMNew subject after splitting |
|
12/11/2018 10:58 AM | |
Joined: 10/11/2006 Last visit: 2/8/2023 Posts: 5418 Rating:
|
Hello, with basic positioner, it is described in chapter 8.8.8 8.8.8 Travel to fixed stop https://support.industry.siemens.com/cs/ww/en/view/109757573 General info, when you use TO (Techology object; S7-1500). 4.18 Travel to fixed stop |
With best regards, |
|
Follow us on