12/4/2024 12:08 PM | |
Joined: 7/19/2022 Last visit: 1/15/2025 Posts: 433 Rating: (71) |
Hello ShreyasM, In the S7-1500 H the device equivalent to the CP 443-1 is the CP 1543-1 (Communications processor CP1543-1) To be able to use the CP 1543-1 you must have TIA V19 and FW 3.1 of the CPU. As you can see in the New Firmware Version V3.1 for SIMATIC S7-1500 R/H CPUs |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on