4/30/2019 7:41 PM | |
Joined: 9/27/2006 Last visit: 3/27/2025 Posts: 12344 Rating:
|
Hello ara; The partial part number you are providing corresponds to modules of the ET 200AL family. Normally you should be able to find the ET 200AL units in the Profibus catalog of your programming software (TIA Portal v15, for example). The gsd file integrates the IM 157-1 head module for the ET 200AL, the 6ES7141-5A,,,,, modules are part of the gsd file. If your programming sifytware is not up to date, you might need an HSP file. If you prefer, the gsd file for the ET 200AL is available here: PROFIBUS GSD files : ET 200AL https://support.industry.siemens.com/cs/ww/en/view/92346281 SIMATIC ET 200AL Distributed I/O system https://support.industry.siemens.com/cs/us/en/view/89254965 You can see this in this extract from the gsd file below: main unit, IM 157-1DP, I/O modules (SM 141-5A... integrted as part of the gsd file. ;-------- <Unit-Definition-List> --------------- GSD_Revision=5 Vendor_Name="SIEMENS" Model_Name="IM 157-1 DP V1.0" Revision = "V1.0" Ident_Number = 0x81A9 Protocol_Ident = 0 Station_Type = 0 FMS_supp = 0 Hardware_Release = "1" Software_Release = "V01.00.00" Info_Text="PROFIBUS Interface modul IM157-1 DP for ET 200AL electronic module\ s; DPV1-slave; degree of protection IP65/67; width 45mm; 2x ET-Connection; 3\ 2 I/O modules; FW-Update via bus; I&M functionality; configuration control via \ plc; firmware V1.0" ------- ;-------------------------------------- ; "8-kanalige Digital-Module Input" ;-------------------------------------- Module="DI 8x24VDC 8xM8" 0x44,0x00,0x00,0x8D,0x40,0x08 110 Ext_Module_Prm_Data_Len = 2 Ext_User_Prm_Data_Const(0) = 0x02,0x00 ;Ext_User_Prm_Data_Ref(1) = 1 ;Eingangsverz. fix 3.2ms da kein Map2.1 entfaellt Parameter ;Ext_User_Prm_Data_Ref(1) = 2 entfaellt, da nicht immer sicher ausloesbar Ext_User_Prm_Data_Ref(1) = 72 Info_Text = "6ES7 141-5BF00-0BA0 Digital input module DI 8x24VDC, 8xM8; degree \ of protection IP65/67; width 30mm; input delay 3ms; input type 3 (IEC 61131); c\ onfigurable diagnostics" EndModule Hope this helps, Daniel Chartier |
5/2/2019 9:05 AM | |
Posts: 15 Rating:
|
These short links might be useful: For PROFIBUS GSD files http://www.siemens.com/profibus-gsd and for PROFINET GSD files http://www.siemens.com/profinet-gsd. |
5/9/2019 9:43 PM | |
Posts: 11 Rating:
|
Hi Mr.Dchartier & MTX500, Thanks a lot, my problem get solved by installing the HSP of TIA V13, as per your suggestion Thanks, ARA12 |
Follow us on