6/16/2015 12:36 PM | |
Joined: 2/28/2015 Last visit: 5/13/2021 Posts: 8 Rating:
|
In general, for small logic optimization, analysis and synthesis I recommend you Logic Friday 1. It’s freeware and you can download it from: http://www.sontrak.com/downloads.html. Another freeware option is SimpleSolver: http://www.simplesolverlogic.com For your application, try to use edge triggered functions like NAND gate or the Wiping Relay with inverted Trg input. For more info double-click the function and then Help or go straight to help and look for the function in the content. For Edge Triggered Wiping Relay: put 3s in TL and 0,1-0,2s in TH (don't care). I think you also need to memorize the status with a Latching Relay or a Pulse Relay.
|
Last edited by: aquariusf at: 6/16/2015 12:55:51 PM |
|
This contribution was helpful to
2 thankful Users |
6/17/2015 12:11 PM | |
Joined: 1/24/2014 Last visit: 11/14/2023 Posts: 119 Rating:
|
is there any manual for guide to use these software ??? |
Follow us on