Industry Online Support
Technical Forum
4/26/2014 11:45 AM | |
Posts: 10 Rating:
|
I can not figure out how to connect "PID_Compact_1" and "Axis_1" anyone knows this ? |
4/26/2014 1:00 PM | |
Posts: 5225 Rating:
|
Hi-ya, Your description does not say much.. what do you want to do? (please select one) a) create a motion control axis b) create a PTO pulse that you use as a reference instead of using an analog c) do PID control using pulse width modulation d) create a PWM signal as reference (see b) e) something else.. (please explain more clearly) I think you a want to drive a stepper motor or servo motor. This falls under (a) or (b) where I personally use the PDF document entitled: "STEP 7 S7-1200 Motion Control V11 SP2" Let us know if this helps OR give more information. |
4/26/2014 5:55 PM | |
Posts: 10 Rating:
|
BTW . my sensor is mounted on the actuators moving part. in the video it's mounted the actuators stationary part. |
Follow us on