Industry Online Support
Technical Forum
6/26/2011 6:44 AM | |||
Joined: 2/1/2011 Last visit: 1/18/2025 Posts: 14 Rating:
|
According to below detalis, can i transfer or download My project to panel KTP1000 Basic DP? My devices are:
http://support.automation.siemens.com/WW/view/en/19109408 Notes on the USB PC adapter (6ES7972-0CB20-0XA0) The USB PC adapter provides an MPI/DP interface via the PC's USB interface. More information is available in the manual in Entry ID: 16983464. This cable is released only for the devices below for project transfer and OS updating.
Hossein Shahrooz |
||
6/27/2011 11:10 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed in the following thread Need help regarding programming HMI KTP1000 by means of PC Adaptor. Best regards O_Moderator |
Follow us on