9/23/2014 3:37 AM | |
Posts: 11 Rating: (0) |
Hello, I need some help with comissioning a servo motor my siemens 810d controlled mill. Below are my machine specifications Simodrive 611 e/r module 6SN1145-1BA01-0BA1 Sinumerik 810D CCU3 V6.4 6FC5447-0AA00-0AA1 PCU20 V6.02.46 Shopmill V6.02.21 I am trying to set up a 4th axis indexer using a 1FK6042-6AF71-1AH0 servo motor. The machine builder sent me the set up procedure manual, however I do not have the motor boot file for this motor, I beleive I could also build the boot file based on the motor converter setting data but I do not have this information as well. I accidentaly deleted the old motor boot file and can not figure out how to make a new one. I have attached the machine builders install instructions. Any help would be apreciated thanks Eric AttachmentSiemens 810D with PCU20rev.pdf (87 Downloads) |
Last edited by: artisan7471 at: 9/23/2014 3:41 AM |
|
9/24/2014 9:55 AM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
|
10/8/2014 6:03 AM | |
Posts: 11 Rating: (0) |
So I guess I need to hire a technition to have this done, nobody seems to know how to do this? |
10/17/2014 4:32 AM | |
Posts: 11 Rating: (0) |
Where can I get HMI advanced? Also what is the cost on this? thanks |
Follow us on